show the entry list
3ZS23 SwitchES Power: Advices for a common installation of Power and SIRIUS ES Software
Part number:

QUESTION:

What has to be considered during the common installation of SwitchES Power and Siemens IA&DT Software Products (for instance STEP7, SIRUS ES)?



ANSWER:

Installation sequence:
The installation of Switch ES Power has to be done before the installation of further SIRIUS ES software products. Otherwise a component fault could occur (50::0033).

Background:
The setup of Switch ES Power installs its version of components without having controlled an already installed more recent version. Thereby, an incompatible installation of SIRIUS ES platform components can occur.

Solution:
First of all, all Siemens IA&DT software products (see uninstalling sequence) followed by Switch ES Power have to be uninstalled. Then, Switch ES Power has to be installed primary followed by further Siemens IA&DT software products.


Uninstalling sequence:
Please consider that Switch ES Power has to be uninstalled after uninstalling all remaining Siemens IA&DT software products. Otherwise uninstalling problems of Siemens IA&DT software products could occur.

Background:
If Switch ES Power is installed as first Siemens IA&DT software product on the target system and uninstalled before all other Siemens IA&DT software products (which Siemens IA&DT setup frames use), the registry entries will be deleted under:HKLM\Software}Siemens\Shared Tools. This means that the UninstallString is not available any more and an uninstalling of further Siemens products can not occur.

Solution:
Incomplete uninstalled products have to be installed again and subsequently to be uninstalled.

 

 Entry ID:27090454   Date:2012-03-15 
I regard this article....as helpfulas not helpful                                 
related links
SITRANS LR560 (Foundation Fieldbu ...
SITRANS LR560 (PROFIBUS PA) - Qui ...
SITRANS LR560 (PROFIBUS PA) - Qui ...
SITRANS LR560 (Foundation Fieldbu ...
SITRANS LR250 (FF) - Quick Start ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour