show the entry list

Mobile Panels -- Operation and maintenance -- Saving data 
How do you backup/restore with a Windows-based panel? 
How do you have csv archive files exported from WinCC flexible RT or a panel displayed graphically on the PC? 
How can you make a project backup from an operator panel? 
Exporting a password list without path specification 

How do you backup/restore with a Windows-based panel?Go to beginning
Part number:

Instructions
There are two option for making a backup of the configuration of a Windows-based panel without having to access the source data of ProTool or WinCC flexible:

1. Backup/Restore with ProSave
2. Backup/Restore with a memory card

Entry ID: 58876345 includes a description of how to do a backup/restore from a Comfort Panel without SIMATIC WinCC V11.

If you want a retransfer whose file can be edited, you must use the Retransfer function in ProTool or WinCC flexible. This is only possible with panels that support this function and in which retransfer is enabled in the transfer settings. Refer to Entry ID: 21907703 to see which panels support retransfer.

1. Backup/Restore with ProSave
With ProSave you have a convenient option of central archiving even without ProTool or WinCC flexible. This provides you with a quick way of starting up again after a system failure or replacement of devices. The backed-up data is transferred to the new target device and the original status thus restored.

Entry ID: 21907703 includes in Attachment 2 a list of all the operator panels that support backup/restore with ProSave.

It is not possible to load and edit a backup file in ProTool or WinCC flexible. The file can only be reloaded to the original or another panel via a restore with ProSave.

Note
Operator panel TP070 does not support backup/restore with ProSave.
 
No. Procedure
1

Preparations for Backup/Restore

  • Depending on the operator panel, you can use one of the following connections for a backup/restore with ProSave:

    - Serial (over RS232/PPI multimaster cable) 6ES7 901-3CB30-0AX0
    - Serial (over USB-PPI cable) 6ES7 901-3DB30-0XA0
    - Serial (over RS232 / zero modem cable) *)  6ES7 901-1BF00-0XA0
    - MPI / PROFIBUS DP
    - Ethernet
    - USB (host-to-host cable) information in Entry ID: 19142034

    *)You can create the zero modem cable (6ES7 901-1BF00-0XA0) yourself. More information is available in Entry ID: 21401061.


    Fig. 01
     
  • If you do not have ProTool or WinCC flexible, you can also download ProSave independently - see Entry ID: 10347815. ProSave allows a complete backup directly from the panel including the configuration. The backup created can then be loaded back into the original or an identical device.
  • Connect the PC with the panel and put it the panel in Transfer mode. If not configured, you can put the panel in this mode by switching the power off and on again. For this you must select and hold the Transfer button when you restart the panel.

    Now the panel is in Transfer mode and ready for backup/restore.

If you want to make a restore, you can jump directly to Point 3 "Restore".

2

Backup

  • Open ProSave and select the correct panel in the "General" tab.


    Fig. 02
     
  • Select the connection between the PC and the panel, serial (over RS232 / zero modem cable), for example.
     
  • Define the connection parameters, for example COM1 with a baud rate of 38400 for the serial connection.

    Note:
    In USB connections (host-to-host cable) and serial connections over USB-PPI cable, you cannot define additional connection parameters.
     
  • Switch to the "Backup" tab, select the path and specify a file name, "C:\panel.psb", for example. Under the "Data type" you define the type of backup to be created.

    Note:
    The file extension ".psb" is necessary, because only this file type can be loaded for a restore.


    Fig. 03
     
  • When everything is set, you trigger the backup procedure with "Start Backup".

    Note:
    If the connection is interrupted, it might be because another software, virus scanner or power management, for example, is accessing the COM interface. Therefore, make sure that any such software is terminated before restarting.
     
  • Once the backup has been completed, the file created can now be loaded back into a device of the same type or back into the original device, as required.
3 Restore
  • First put your panel in Transfer mode as described in Point 1 and set up the connection to the PC.
  • Select the appropriate operator panel and connection type in the "General" tab - see Fig. 02.
  • If possible, define the connection parameters.
  • Switch to the "Restore" tab in ProSave.
  • Open your ".psb-file" and transfer the loading procedure by clicking "Start Restore".


    Fig. 04
     
  • After successful transfer of data to your panel, this is now ready to be integrated in your system after startup.

    Note:
    The panel has exactly the same connection parameters as the panel from which the backup originates. Make sure that both panels are not in the same system, in order to avoid connection problems.

2. Backup/Restore with a memory card
During saving (backup), the operating system, applications and data are copied from the internal flash memory of the operator panel to the memory card.

When you restore, the flash memory of the operator panel is deleted after a prompt. Then the data backed up on the memory card is copied to the internal flash memory.

Requirements

  • The operator panel supports the Backup/Restore function.

  • A memory card is available in the operator panel with sufficient free space.

Which operator panels support backup/restore with a memory card are given in Entry ID: 21907703.

Use of the backup/restore function depends on the operator panel. In the following we will be considering operator panels of the 177, 277 and 377 series. For other operator panels - in particular for older operator panels - please refer to the relevant manuals for the procedure.
 
No. Procedure
1 Preparation
  • Start the operator panel and open the "Control Panel".
  • Slot the memory card into the operator panel.
  • Open the "Backup/Restore" menu in the "Control Panel".


Fig. 05

If you only want to make a restore, you can jump directly to Point 3 "Restore".

2 Backup
  • Click the "Backup" button in "Backup/Restore" dialog.


Fig. 06

Note
Figure 06 shows the "Backup/Restore" dialog of an operator panel with Windows CE 5.0.

2.1

Backup - operator panels with one interface for memory cards

With operator panels with only one interface for memory cards, the memory card is automatically searched for.

a) Memory card detected
If the backup is successful, the "Backup successfully completed." dialog opens.

  • Acknowledge the dialog with "OK".

If there is already an old backup on the memory card, a message is issued on the operator asking whether or not you want to delete the old backup.

  • Acknowledge the message with "Yes" if you want to delete the old backup and create a new one.
  • Acknowledge the message with "No" if you do not want to delete the old backup and want to interrupt the current backup procedure. Acknowledge the interrupt with "OK".

A warning is displayed if the available memory is insufficient.

  • Use an appropriate memory card or delete all the unnecessary data in the Windows CE Explorer.

b) Memory card not detected
If there is a defective memory card in the operator panel, or none at all, then the following message is displayed.


Fig. 07

  • Click "OK" to close the warning. 
  • Click "OK" to acknowledge the "Backup interrupted" message.
  • Repeat the procedure using an appropriate memory card.
2.2

Backup - operator panels with multiple interfaces for memory cards

In the case of operator panels with multiple interfaces for memory cards, you can select the memory card explicitly on the operator panel - see Fig. 8.

  • In the list box - see Fig. 08 - you select the required memory card and then click the "Start Backup" button.

Warning - possible loss of data!
When you first use a memory card, the operator panel prompts you to format it.

  • Click the "ESC" button to abort the formatting procedure.

If no memory card is slotted or the memory card is defective, then no memory card is displayed.

  • In this case, slot a memory card that functions into the operator panel.


Fig. 08

If the message is displayed indicating that a higher storage capacity is required, then proceed as follows:

  • Click "OK" to acknowledge the message and thus interrupt the backup.
  • Slot a memory card with the higher storage capacity into the operator panel.
  • Start the backup again.

If there is already an old backup on the memory card, you get a message asking you whether this backup should be overwritten.

  • Acknowledge the message with "Yes" if you want to delete the old backup and create a new one.
  • Acknowledge the message with "No" if you do not want to delete the old backup and want to interrupt the current backup procedure. Acknowledge the interrupt with "OK".

The backup is completed when the "Backup successfully completed..." message is displayed.

  • Acknowledge the message with "OK".
  • Remove the memory card from the operator panel.
3 Restore
  • Click the "Restore" button in the "Backup/Restore" dialog - see Fig. 06.


Fig. 09

Note
Figure 09 shows the "Backup/Restore" dialog of an operator panel with Windows CE 3.0.

3.1 Restore - operator panels with one interface for memory cards
In the case of operator panels with only one interface for memory cards, you can do a restore only via that interface.

a) Memory card detected
If the memory card is detected, a message is displayed asking whether the restore procedure should be continued. Here, all the data of the flash will be deleted on the operator panel.

  • Acknowledge the message with "Yes" if you want to start the restore.
  • Acknowledge the message with "No" and then the following message with "OK" if you want to abort the restore.

Once the flash has been deleted and the Windows CE image has been successfully restored, you must reboot the operator panel.

  • Acknowledge the message with "OK".

    Note
    Do not remove the memory card from the operator panel during the restart!

As soon as the restore has been successfully completed, a message is displayed prompting you to remove the memory card from the operator panel.

  • Remove the memory card from the operator panel.
  • Acknowledge removal of the memory and reboot with "OK".

b) Memory card not detected
If there is a defective memory card in the operator panel, or none at all, then the following message is displayed.


Fig. 10

  • Slot an appropriate memory card into the operator panel and acknowledge this with "OK" if you want to execute the restore.
  • Click the "X" if you want to abort the restore procedure.
3.2 Restore - operator panels with multiple interfaces for memory cards
In the case of operator panels with multiple interfaces for memory cards, you can select the memory card explicitly on the operator panel - see Fig. 1.
  • In this case, you select the memory card that contains the backup.

If no memory card is slotted or the memory card is defective or the memory card contains no backup, then no memory card is displayed.

  • In this case, slot a memory card that functions and which contains a backup of the operator panel into the operator panel.

Only storage media containing a backup is detected.

  • Then click the "Start Restore" button.

If multiple external storage media with a backup are slotted on one operator panel, data restore is not possible.

  • Remove all the external storage media units that contain a backup and are not relevant and then click the "Refresh" button.
  • Alternatively you can abort the restore procedure by clicking the "Cancel" button.


Fig. 11

Once the data to be restored has been checked, a prompt is displayed querying whether you want to start Restore and in doing so whether you want to delete all the data on the flash.

  • Acknowledge the message with "Yes" if you want to start the restore.
  • Acknowledge the message with "No" and then the following message with "OK" if you want to abort the restore.

The restore is completed when the "Restore successfully finished..." message is displayed.

  • Click "OK" to acknowledge the message and restart the operator panel.

Additional Keywords
OP73, TP070, TP170, TP177, Mobile Panel170, Mobile Panel177, Mobile Panel277, OP77A, OP77B, TP170A, TP170B, TP177A, TP177B, OP170B, OP177, TP270, TP277, OP270, OP277, MP270, MP270B, MP277, MP370, MP377, Linux-based operator panels

How do you have csv archive files exported from WinCC flexible RT or a panel displayed graphically on the PC?Go to beginning
Part number:

Introduction:
In the Runtime mode of WinCC flexible, you can store tag values in archives and evaluate them later. These tag archives are difficult to read outside the panel and cannot be evaluated graphically without WinCC.

Solution:
The Excel file "WCf-ArchivViewer" provides a graphical user interface via VBA script, which provides numerous operator input options. In the "WCf-ArchivViewer", all you have to do is enter the names of the archive files. Here, when reading in the archive files, it is also possible to select just the data you require. The "WCf-ArchivViewer" provides numerous options for evaluating the archive files, e.g.:

  • Graphical user interface as pivot diagram
  • Evaluation using pivot table
  • Compression of time values (removal of time buttons)
  • Compression of value display (mean value, maximum value, buzzer, ...)
  • Time selection (year/month/day/hour/minute)
  • Change the diagram types
  • Selection of desired trends

Attachment 1: WCf_ArchivViewer.xls ( 52 KB )

Sample program:
The example describes how the tag archives created can be evaluated in the "WCf-ArchivViewer" without interrupting their recording.
The "Temp_1" tag archive has been created in the example, in which the tag "test_tag" is archived.
The archive is stored on a USB stick on the panel. It should be possible to evaluate the archive at any time with the "WCf-ArchivViewer" without interrupting recording of the values.
For this, you must integrate the panel into an existing local network. A detailed description of this is available in Entry ID: 13336639.

The sample project contains a script that you have to change to suit your configuration. Here you change your paths for the storage locations.


Fig. 01

Procedure for evaluating the archive on the PC:

  1. When you first start the Excel table, the following query is displayed. Click on the "No" button.

    Fig. 02
  2. On the operator panel you use the "Copy to PC" button to copy the archive file from the panel to the computer specified.
  3. Place the "WCf-ArchivViewer" with the archive files in a folder to start evaluation.
  4. Open the "WCf-ArchivViewer" and enter the archive file "Temp_10.csv" in the second row (under File name). In the left column, you enter a "1" (under Enable) to active the archive.
    Then lick on the "Read in archive data and create graphics" button. Acknowledge the dialog displayed with "Yes".
    Now, you can visually evaluate the recorded values without needing any component of WinCC flexible.


Fig. 03

Note:
Another option is to use Sm@rtService.
Using Sm@rtService you can connect to the operator panel and download individual files to your local PC and then evaluate them.

Attachment 2: Archiv_Viewer_Beispielprojekt.zip ( 2028 KB )
 
Components Product and version designation
HMI software WinCC flexible 2008 SP1
HMI Panel MP 277 10" Touch
Office software MS Excel 2003 (German version and Regional Options)

Runnability and test environment:
The tables above list the components that have been used to create this entry and verify the functions described.

How can you make a project backup from an operator panel?Go to beginning
Part number:

Instructions:
Based on a number of examples we will demonstrate how to make data/project backups with the various operator panels.

Line / graphics operator panels:
You can use the service tool ProSave with the line operator panels TD 17, OP 7, OP 17, C7-633, C7-634 and graphics operator panels OP 27, TP 27, OP 37, TP 37.
With ProSave you can store the entire contents of the OP's memory in one file (Backup) and then reload this file onto the operator panel (Restore).
Please use ProSave V7.3 onwards for Backup and Restore.
The service tool and more information on it are available in Entry ID 10347815.

Note:
Backup files cannot be edited.

Please refer to the table that you can download in Entry ID 21907703 for which line and graphics operator panels support Backup/Restore with ProSave.

Graphics operator panels:

  • Backup:
    Graphics devices have another option for making a backup.
    If you have integrated the default page "Z_Backup" in your ProTool project or have assigned the "Backup / Restore Module" function to a button, then you can use this function to make a backup on a memory card.

The following memory cards are released for use in graphics operator panels:

  • 6ES7 952 – 1KL00 – 0AA0 2 MB
  • 6ES7 952 – 1KM00 – 0AA0 4 MB
  • 6ES7 952 – 1KP00 – 0AA0 8 MB
  • 6ES7 952 – 1KS00 – 0AA0 16 MB
     
  • Restore:
    Proceed as follows to transfer a configuration backed up on a memory card back to the operator panel.
No. Procedure
1 Slot the memory card with the data to be downloaded into the operator panel.
2 Start the operator panel.
The operator panel recognizes the slotted memory card at startup.
3 Acknowledge the security prompt about running a restore with OK.
The operator panel downloads the stored data (firmware/project/data records) into the internal memory during startup.
After ending the Restore procedure the operator panel goes into Transfer mode.
4 Remove the memory card from the operator panel to avoid another restore being made from the memory card the next time you start the operator panel.
5 Start loading the project by interrupting the Transfer mode with OK.

Windows CE operator panels:
You can use the ProSave service tool for Windows CE operator panels.
The service tool and more information on it are available in Entry ID 10347815.

Another way of doing a Backup/Restore is via the Control Panel of the operator panel*).
For this you need a memory card with sufficient capacity. For this you open the "Control Panel" or "Loader" on the operator panel.
In the "Control Panel" you select the menu item "Backup/Restore". Via this menu item you can execute the Backup/Restore function.

*) Note:
Refer to the relevant device manual for which devices support Backup/Restore and for detailed instructions.

Further Information:
 
How do you backup/restore with a text-based or graphics-based panel? Entry ID: 26588748
What transfer options are available in the various operator panels? Entry ID: 19109408
Which HMI operator panels support retransfer of the configuration? Entry ID: 21907703
Error message during retransfer: "Could not find the pdz file". Entry ID: 13393218

Exporting a password list without path specificationGo to beginning
Part number:


QUESTION:
When exporting a password list, where is the generated file stored?

ANSWER:
When configuring the function "Import/Export Passwords", you have to specify the file name for the password list to be imported/exported. By specifying the path you can also define the storage location of the file with this parameter.
With the path specification "\storage card\file name", for example, the password list is stored on the slottable flash card of the OP. If you do not specify a path when exporting a password list, storage is made on the internal flash.

More information is available in the online Help of ProTool/Pro.


 Entry ID:26348329   Date:2012-05-18 
I regard this article....as helpfulas not helpful                                 






























related links
SIMATIC HMI HMI device OP 73, OP ...
SIMATIC HMI HMI Device TP 177A, T ...
SIMATIC HMI HMI device MP 277 (Wi ...
SIMATIC HMI Mobile Panel 170
SIMATIC HMI HMI device MP 177 (Wi ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour