show the entry list

Multi Panel -- Setting up systems -- Transferring projects  
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS? 
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel? 
What transfer options are available in the various operator panels? 
How do you back transfer the projects of an operator panel and what should you watch out for? 
How do you simulate the system keyboard via K or F-keys? 
How can you transfer a WinCC flexible project via Ethernet to a Windows-based panel? 

How can you transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS?Go to beginning
Part number:

Description
The attached PDF document informs you about the settings needed to transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS.


Fig. 01

The document describes the following settings...

  • On the operator panel.
  • On the configuration PC.
  • In WinCC (TIA Portal).

Download
Documentation
 
WinCC V11 (TIA Portal) Project transfer

WinCC_V11_Panel_MPI_DP_Transfer_en.pdf ( 961 KB )

Note on security
Caution
The functions and solutions described in this article confine themselves predominantly to the realization of the automation task. Furthermore, please take into account that corresponding protective measures have to be taken in the context of Industrial Security when connecting your equipment to other parts of the plant, the enterprise network or the internet. More information can be found in Entry ID: 50203404.

Additional Keywords
Download, Transfer, Load, Control Panel, Channel, Remote Control, Commissioning, Project transfer, Bus address, Transmission rate, Device configuration, Bus parameters, Network settings, Network view, Connection, Nodes, PG/PC interface, Interface configuration

When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?Go to beginning
Part number:

Description:
After project transfer to an operator panel, the configuration PC crashes or no longer works reliably.
This behavior can be caused by using the "Kaspersky" virus scanner. It occurs as from version V6.0. The crash is due to a security update from "Kaspersky".

Remedy:
The "Kaspersky" virus scanner is not released for WinCC flexible. You can remedy this behavior as follows.

  1. Uninstall or deactivate the "Kaspersky" virus scanner.
  2. Release the processes "Hmies.exe" and "TransferTool.exe" in the virus scanner.

Note:
More information on the topic of "Virus scanners with WinCC flexible" and on the compatibility of tested virus scanners is available in the WinCC flexible help system under:
 "First Steps > Installation Guide > Installation > Installing WinCC Flexible > Antivirus tools".

What transfer options are available in the various operator panels?Go to beginning
Part number:

Transfer options
Attachment 1 lists the operator panels and their transfer options.

Attachment 1: Projecttransfer_V1_2_e.pdf ( 17 KB )    

USB host-to-host cables
More information on the topic of "USB host-to-host cables" is available in Entry ID: 19142034.

Application of adapters and cables
Attachment 2 indicates for each operator panel the plug-in cable required for the following applications:

  • Process coupling
  • Download (update operating system, project, ...)
  • Booting (filling in the case of a missing or damaged operating system)

Attachment 2: Panels_connecting_cables_V1_2_e.pdf ( 29 KB )  

Notes on USB PC adapter (6ES7972-0CB20-0XA0)and USB A2 PC adapter (6GK1 571-0BA00-0AA0)
The USB PC adapter/USB A2 PC adapter provides an MPI/DP interface through the PC's USB interface. More information about the USB PC adapter is available in the manual in Entry ID: 16983464 More information about the USB A2 PC adapter is available in the manual in Entry ID: 68849363
These cables are released only for the devices below for project transfer and OS updating.

  • OP 73
  • OP 77 A
  • TP 177 A
  • KTP600 Basic Color DP
  • KTP1000 Basic Color DP

Using USB RS232 adapters and USB Ethernet adapters
When using the RS232/PPI Multi-Master cable, zero modem cable or Ethernet connections, you can only use the "real" interfaces for project transfer.
"Real" interfaces are interfaces without implementation via USB. This means that you cannot use any "USB to serial" or "USB to Ethernet" adapters.

Additional Keywords
Project transfer, Project download, WinCC flexible, Transfer cable, ProTool, RS 232, PC/PPI cable, PC PPI cable, RS 485, Com Text, Cables, USB adapter

How do you back transfer the projects of an operator panel and what should you watch out for?Go to beginning
Part number:

Contents:
In this FAQ we describe how to back transfer projects, which operator panels support this function and what you should pay attention to.

Please follow the instructions in the PDF file (Attachment 1).
The following points are covered in the document.

1. General Information
    1.1 Using back transfer
    1.2 Advantages of back transfer
    1.3 Requirements for back transfer

2. Procedure
    2.1 Project transfer and back transfer

3. Frequently Asked Questions
    3.1 Why is the message "Could not find the pdz file" displayed?
    3.2 How do you determine whether a back-transferred file is on the panel?

Attachment 1: Back_transfer_description_e.pdf ( 491 KB )

Requirements for back transfer
Attachment 2 lists the operator panels and indicates which HMI software is required to transfer projects and which operator panels permit back transfer of the configuration file from the operator panel.

Furthermore it also shows from which operator panels you can do a backup/restore via ProSave and which operator panels permit backup/restore to/from external memory cards.

Attachment 2: Back_transfer_devices_e.pdf ( 60 KB )

Note:
A comparable method of saving projects is with Backup/Restore. More information on this topic is available in the following Entry IDs: 28928853, 26588748 and 213262.

Keywords:
Panel, WinCC flexible, Store, 13393218, 5672699

How do you simulate the system keyboard via K or F-keys?Go to beginning
Part number:

Instructions:
The system keyboard can be simulated using the SimulateSystemKey function from WinCC flexible 2005. The function is particularly useful if the operator panel does not possess a separate number block or if, for example, you use an OP177B with a touch/button combination.

By "simulating" the system keyboard, the operator, on the OP 177B for example, does not necessarily have to use the touch screen (if his hands are dirty) to set or enter values on the panel.

In this example, the "number block" was configured to the following function keys in the "Template" screen on an OP 177B (see Fig. 01).


Fig. 01

In the relevant screens you can then choose whether to use the keys, which have been configured in the "Template" screen", "locally" ("Use global assignment").


Fig. 02
 
No. Procedure
1

Click the function key to which you wish to assign the "SimulateSystemKey" function and open the key properties.

2

You can find the "SimulateSystemKey" function in the "Keyboard" system function.

3 The system key which is being simulated can be selected under the "system key" parameter.


Fig. 03

4 Runtime control:
With reference to the attached sample program, you can use the "TAB button" (K2) to switch to the individual "I/O fields".
Click "Enter" (K10) to apply the values which have been input.

All the available "functions" are listed in the file below.

Attachment 1: SystemKeys.pdf ( 10 KB )  

The attached download contains the archived WinCC flexible 2005 project with the functions described above.

Attachment 1: SimulateSystemKey.zip ( 1745 KB )

Runnability and test environment:
The example can be used on all the CPU types of SIMATIC S7-300, S7-400 and WinAC.
The following table lists the components that have been used to create this entry and verify the functions described.
 
Component Product and version designation
PC operating system Microsoft Windows XP SP2
Standard tools -
Engineering tools -
HMI software WinCC flexible 2005 SP1
HMI devices OP 177B
Controllers -
Table 1: Creation environment of the download attached

How can you transfer a WinCC flexible project via Ethernet to a Windows-based panel?Go to beginning
Part number:

Description
The document below informs you how to transfer a WinCC flexible project to a Windows-based panel using Ethernet.

Contents

1 Transfer via Ethernet from a Configuration PC with Windows 7
   1.1 Instructions
   1.2 Settings on the Operator Panel
   1.3 Settings on the Configuration Computer
      1.3.1 Non-integrate Project
      1.3.2 Integrated Project
   1.4 Checking the Ethernet Connection
      1.4.1 Checking the Connection to the Panel
      1.4.2 Checking the Settings on the Operator Panel
   1.5 Settings in WinCC flexible
      1.5.1 Non-integrated Project
      1.5.2 Integrated Project
2 Transfer via Ethernet from a Configuration PC with Windows XP
   2.1 Instructions
   2.2 Settings on the Operator Panel
   2.3 Settings on the Configuration Computer
      2.3.1 Non-integrate Project
      2.3.2 Integrated Project
   2.4 Checking the Ethernet Connection
      2.4.1 Checking the Connection to the Panel
      2.4.2 Checking the Settings on the Operator Panel
   2.5 Settings in WinCC flexible
      2.5.1 Non-integrate Project
      2.5.2 Integrated Project

Download

23800567_WinCC_flexible_Ethernet_Transfer_en.pdf ( 1725 KB )

More information is available in the following entries
 
Topic Entry
Project transfer (released cables,...) Entry ID:
19109408
Communication between SIMATIC station and panel in the following manuals:
"WinCC flexible 2005 Communication Part 1"
"WinCC flexible 2005 Communication Part 2"
Entry ID:
18797552
Entry ID:
18797249
Network connection with DNS server Entry ID:
13336639
OS update with Ethernet (not possible with all panels) Entry ID:
19701610

Keywords
Transfer, Ethernet, Windows XP, Windows 7

 Entry ID:26117866   Date:2013-05-03 
I regard this article....as helpfulas not helpful                                 






























related links
How can you transfer a WinCC flex ...
How can you transfer a WinCC flex ...
SIMATIC HMI WinCC flexible 2008 W ...
How can you make a project backup ...
SIMATIC HMI HMI Device TP 177A, T ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour