show the entry list
ASIsafe -- Produktinformationen -- Systembeschreibung
3RK1105 AS-i Safety monitor: Behavior when the bus or the connected devices show faults
3RK1105 AS-i Safety monitor: Purpose of terminal FE (Functional Earthing)
3RK1105 AS-i safety monitor: Does the ASi-monitor switch off if the CPU starts up with CP343-2 ?
DP/AS-i F-Link: The inputs of the ASIsafe slaves which are connected via DP/AS-i F-Link are zero in the failsafe program
3RK1105 AS-i Safety monitor: Purpose of terminal FE (Functional Earthing)
Part number:

QUESTION:

What is the purpose of terminal FE (Functional Earthing) with the 3RK1105 AS-i Safety monitor?

Is it necessary to connect this terminal "FE" to earth (ground) or can one leave it unconnected ?
 

ANSWER:

Functional Earthing "FE" has following meaning:
Earthing of a location in an electrical system or switchboard or equipment which is required for another purpose than for protection against electrical shock

Connecting the protective earth conductor to the terminal "FE" kann remain undone if the terminal M is connected to earth very proximate to the device.

 Entry ID:25463110   Date:2007-05-14 
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
Themen
Help
Online Help
Guided Tour