show the entry list
Does the SITRANS LR250 have built-in diagnostic capabilities and failure reporting?
Part number:

QUESTION:Does the SITRANS LR250 have built-in diagnostic capabilities and failure reporting?

ANSWER:  Yes, device failures can be detected on the network as an alarm, and numerous parameters record diagnostic data which can then be viewed locally on the display or remotely over a network. Maintenance features are also included whereby the user can set a timer in the device to automatically notify in the future when maintenance is required.

 Entry ID:25436500   Date:2007-05-08 
I regard this article....as helpfulas not helpful                                 
related links
Does the SITRANS LR 200 have buil ...
Does the SITRANS LR 300 have buil ...
Is the SITRANS LR250 safe to operate?
SITRANS LR250 (HART) - Instructio ...
SITRANS LR250 (HART) - Instructio ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour