show the entry list
ASIsafe -- Produktinformationen -- Systembeschreibung
3RK1105 AS-i Safety monitor: Behavior when the bus or the connected devices show faults
3RK1105 AS-i Safety monitor: Purpose of terminal FE (Functional Earthing)
3RK1105 AS-i safety monitor: Does the ASi-monitor switch off if the CPU starts up with CP343-2 ?
DP/AS-i F-Link: The inputs of the ASIsafe slaves which are connected via DP/AS-i F-Link are zero in the failsafe program
3RK1105 AS-i safety monitor: Does the ASi-monitor switch off if the CPU starts up with CP343-2 ?
Part number:

QUESTION:

Does the ASi-monitor switch off if the CPU starts up with CP343-2 ?

ANSWER:

The ASi-monitor does not switch off if the CPU starts up with CP343-2 which means switching from STOP to RUN.
Either, from RUN to STOP the monitor does not switch off.

If, however, the CPU control voltage is turned off, also CP343-2 is out of supply voltage.
Then the monitor switches off due to ASi-master failure.

 Entry ID:25435435   Date:2007-05-08 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour