|
Instructions: For transfer of a WinCC flexible configuration via MPI or PROFIBUS you must make settings on the Windows-based panel and on the configuration PC.
Note:
- Direct transfer from the PC to the Windows-based panel via a PC adapter (RS232 -> MPI/PROFIBUS, USB -> MPI/PROFIBUS) is not supported.
- Project transfer to a Micro Panel is not possible, because a Micro Panel doesn't have an MPI or PROFIBUS interface.
- If you wish to integrate your configuration PC into an existing MPI/PROFIBUS network, you must transfer the bus settings of the available MPI/PROFIBUS subnet. Please note that the bus address of the PC in the MPI/PROFIBUS subnet must be unique.
Settings on the operator panel The figures below are from the MP277. The illustrations might differ from operator panel to operator panel, because not all the functions are available for each operator panel.
| No. |
Procedure |
| 1 |
Settings in "Control Panel" Open the Transfer dialog in the "Control Panel".
 ( 65 KB )
Fig. 01 - Control Panel (MP277)
The MPI/PROFIBUS transfer is enabled under "Channel 2". For this you set Channel 2 to "MPI/PROFIBUS". For Channel 2 you also set a check mark for "Enable Channel" and if you wish, "Remote Control".
 ( 4 KB )
Fig. 02 - Transfer Settings
Note: The "Remote Control" option permits automatic termination of Runtime on the panel when transfer is triggered via the development environment of WinCC flexible. The panel then automatically switches to Transfer mode.
Note:
In the case of transfer via a TS adapter with modem you should enable "Remote Control", because otherwise the panel does not switch automatically into the Transfer mode. |
| 2 |
More settings in "Transfer Settings"
- Open the advanced settings by clicking on the "Advanced" button (Fig. 02).
- Define whether the WinCC flexible project is to be transferred via "MPI" or "PROFIBUS".
- Then click the "Properties" button.
 ( 12 KB )
Fig. 03 - S7 transfer settings
|
| 3a |
Version A - MPI |
MPI settings If you wish to transfer a project via PROFIBUS - Version B, then you can skip this point and go directly to Point 3b.
The following dialog (Fig. 04) shows the current MPI bus parameters of the panel.
If the panel is the only master on the bus, then set the check mark for "Panel is the only master on the bus" and assign a unique bus address (Address) for the device.
Note:
If it is not necessarily required by the system to change the other network parameters, you should use the default network parameters given.
These network parameters must match the settings in the SIMATIC station (e.g.: CPU or CP).
 ( 26 KB )
Fig. 04 - MPI bus parameters
Note:
If other masters (panels) are to be connected to the bus, then disable the option "Panel is the only master on the bus".
|
| 3b |
Version B - PROFIBUS |
PROFIBUS settings
If you are using Version A via MPI, you can skip this point and go directly to Point 4.
The following dialog shows the current PROFIBUS parameters of the panel.
If the panel is the only master on the bus, then set the check mark for "Panel is the only master on the bus" and assign a unique bus address (Address) for the device.
Note:
If it is not necessarily required by the system to change the other network parameters, you should use the default network parameters given.
The network parameters must match the settings in the SIMATIC station (e.g.: CPU or CP).
 ( 30 KB )
Fig. 05 - PROFIBUS bus parameters
Note:
If other masters (panels) are to be connected to the bus, then disable the option "Panel is the only master on the bus". |
| 4 |
Close the dialog window
Close all the open dialogs with "OK".
Also close the "Control Panel" and enable the Transfer mode. |
Settings on the configuration PC For communication between panel and configuration computer you must set the bus parameters as on the panel (except for the node address).
| No. |
Procedure |
| 1 |
Open PG/PC interface In the Control Panel of your configuration computer you open the menu "Set PG/PC Interface".
 ( 46 KB )
Fig. 06 - Control Panel
Alternatively you can also open the PG/PC interface via the SIMATIC Manager.
 ( 18 KB )
Fig. 07 - STEP 7 Manager
|
| 2 |
Setting the PG/PC interface
 ( 22 KB )
Fig. 08 - PG/PC interface
For MPI transfer from the PC to the panel you select one of the following settings (CP = communication processor) that you use for the hardware:
| S7ONLINE (STEP 7) |
--> |
CP5512 (MPI) |
| CP5611 (MPI |
| CP5611 A2 (MPI) |
| CP5613 (MPI) |
| CP5613 A2 (MPI) |
| CP5613 FO (MPI) |
| CP5614 (MPI) |
| CP5614 A2 (MPI) |
| CP5614 FO (MPI) |
| CP5611 A2 (MPI) |
For transfer via PROFIBUS you select one of the following interface parameterizations:
| S7ONLINE (STEP 7) |
--> |
CP5512 (PROFIBUS) |
| CP5611 (PROFIBUS) |
| CP5611 A2 (PROFIBUS) |
| CP5613 (PROFIBUS) |
| CP5613 A2 (PROFIBUS) |
| CP5613 FO (PROFIBUS) |
| CP5614 (PROFIBUS) |
| CP5614 A2 (PROFIBUS) |
| CP5614 FO (PROFIBUS) |
| CP5611 A2 (PROFIBUS) |
Note:
If none of the interfaces listed above is shown, you can install interfaces manually by clicking on the "Select..." button in the "Interfaces" "Add/Remove" field. |
| 3a |
Version A - MPI |
| Set interface parameters
If you wish to transfer a project via PROFIBUS - Version B, then you can skip this point and go directly to Point 3b.
- Click the "Properties..." button. (Fig. 08).
- Set the check mark for "PG/PC is the only master on the bus" if no other master is connected in the subnet.
- Change the network-related parameters - except the node address - to match the settings on the panel for MPI (Fig. 4).
- Close the Properties dialog box with "OK".
 ( 8 KB )
Fig. 09 - MPI properties
Note:
The node address must be unique, i.e. it must not be used by any other nodes in the subnet. Please note that the address must not be greater than the highest permissible Highest Station Address (HSA). |
| 3b |
Version B - PROFIBUS |
Interface parameters
If you are using Version A via MPI, you can skip this point and go directly to Point 4.
- Perform the same steps as for the MPI interface parameters (Point 3a).
- The network-related settings for the PROFIBUS communication - except the node address - must match the interface settings on the panel (Fig. 5).
- Close the Properties dialog box with "OK".
 ( 12 KB )
Fig. 10 - PROFIBUS properties
Note:
The node address must be unique, i.e. it must not be used by any other nodes in the subnet. Please note that the address must not be greater than the highest permissible Highest Station Address (HSA). |
| 4 |
SIMATIC NET Diagnostics
- Open the "Diagnostics" to test the MPI/PROFIBUS connection between the PC and the panel.
- Perform network diagnostics for the CP by clicking on the "Test" button.
 ( 13 KB )
Fig. 11 - SIMATIC NET Diagnostics
|
Node address |
Node |
| 10 |
HMI operator panel |
| 2 |
SIMATIC station (e.g.: CPU) |
| 0 |
PG/PC interface (e.g.: CP5512) |
Table 01
Note:
If the operating mode is not "OK", check the hardware and the bus parameters (Points 3a and 3b) in the PG/PC interface. If necessary, check the CPU settings in the Hardware Configuration of the SIMATIC Manager and the settings on the panel.
Note:
More information on error messages is available via Help (see button) in the dialog window under "Error messages > Error message".
In order to determine the current bus parameters of a subnet you can also proceed as described in Point 5:
- If the operating mode or network diagnostics is "OK", then click on the "Read" button. The table shows the bus node that can be reached (Address 10 = Panel).
- Close the open dialogs with "OK".
|
| 5 |
Determine bus parameters
You can skip this point if the operating mode is "OK" in Point 4 and the bus nodes are displayed after read-out.
Set the CP adapter of the interface parameterization to "AUTO" and click the "Properties..." button.
Example:
"S7ONLINE (STEP7) -- > CP5512(AUTO)"
 ( 22 KB )
Fig. 12 - AUTO properties
Start the network identification by clicking on the "Start Network Detection" button.
 ( 9 KB )
Fig. 13 - Network identification
 ( 39 KB )
Fig. 14 - Analysis of the bus parameters
Note:
Via the "Bus Parameters..." button you can have all the relevant bus parameters displayed in detail.
Note: If the bus parameters cannot be determined or a synchronization error occurs, then you should check the following points:
- PROFIBUS or MPI cable (replace where necessary).
- Correct setting of the terminators.
- Bus parameters on the panel and in the PG/PC interface.
- Physical connection between the CP and the panel.
- Power supply of the SIMATIC stations.
- If necessary, compile and transfer the Hardware Configuration in the SIMATIC Manager for all relevant SIMATIC stations (e.g. CPU).
More information is available in the Help of the MPI/PROFIBUS diagnostics in each case. |
Settings in WinCC flexible As an option you can also integrate the WinCC flexible project into a STEP 7 project. The two possible versions are explained in the following table.
| No. |
Procedure |
| 1 |
Create connection
- In the project tree structure under "Communication" you select the "Connections" tab.
- In WinCC flexible you insert a new connection in the menu under "Insert > New Object - Connection".
Alternatively you can double-click an empty field in the table in the "Connections" tab and create a new connection.
 ( 89 KB )
Fig. 15 - Connections
|
| 2a |
Version A - Non-integrated project |
Define parameters If you have created an integrated WinCC flexible project or would like to integrate it into STEP 7, you can skip this point and go directly to Point 2b.
Define the relevant parameters that you have already specified in the panel and in the PG/PC interface. The MPI or PROFIBUS protocol can be defined separately under the option Network > Profile.
For networking with MPI or PROFIBUS you need the interface IF1 B (for panels) or MPI/DP (for PC-based operator panels).
 ( 134 KB )
Fig. 16 - Connection parameters
Note:
If you do not implement an S7-300/400 CPU as communications partner, then change the communication driver.
The following communication drivers that support the MPI or PROFIBUS protocol are available:
- SIMATIC S5 DP (only PROFIBUS)
- SIMATIC S7-200
- SIMATIC S7-300/400
- SIMOTION
|
| 2b |
Version B - Integrated project |
Defining the station You can skip this section and go directly to Point 3 if you do not want to use an integrated project.
If you have not already inserted the project in the SIMATIC Manager, you can do this via the WinCC flexible menu "Project > Integrate in STEP 7...".
- Open NetPro in the SIMATIC Manager. Alternatively you can also open the Hardware Configuration of the HMI operator panel.
 ( 24 KB )
Fig. 17 - Open NetPro
- In the NetPro dialog (Fig. 18) you double-click the HMI MPI/DP interface of the "SIMATIC HMI Station(1)".
- Click on the "Properties..." button in the Properties dialog window of the HMI MPI/DP interface.
- Mark the MPI(1) subnet of the HMI station then click "OK".
Note:
You can use the "New..." button to add more subnets. Note here that the HMI station and associated SIMATIC station must be in the same subnet or connected together via a routing-compatible station. More information on S7 Routing is available in Entry ID: 22255588.
 ( 72 KB )
Fig. 18 - Select station
- Close the dialog window with "OK".
- Save and compile your configuration via the menu "Network > Save and compile...".
- Where applicable, transfer your changed hardware configuration to all the relevant SIMATIC stations and terminate NetPro.
- Via the corresponding subnet you select the station with which the operator panel is to communicate.
 ( 132 KB )
Fig. 19 - Select station
|
| 3 |
Project transfer
- Open the dialog window under "Project > Transfer > Transfer Settings...". Alternatively you can also open the transfer settings via the toolbar (1).
- In the "Transfer Settings" dialog you select the relevant operator panel (2) - only necessary in the case of multiple operator panels.
- Select MPI/DP (3) as the Transfer mode and enter the node address of the operator panel.
Note:
For the possible transfer options please refer to the relevant manual or Entry ID: 19109408.
- With the "Transfer" button (4) you can now transfer your configuration to the panel.
 ( 99 KB )
Fig. 20 - Project transfer
Note:
If you do not want to transfer yet, you can save the settings with "Apply".
With the first transfer of the project to an operator panel you should disable the "Delta transfer" option and enable the "Overwrite password list" option.
Note:
After transfer the panel adopts the parameters set in the "Connections" tab. |
More information is available in the following entries.
| Topic |
Entry |
| Project transfer (released cables,...) |
Entry ID: 19109408 |
Communication between SIMATIC station and panel in the following manuals:
"WinCC flexible 2005 Communication Part 1"
"WinCC flexible 2005 Communication Part 2" |
Entry ID: 18797552
Entry ID: 18797249 |
| Transfer via S7 Routing over MPI/PROFIBUS and Ethernet (as from WinCC flexible 2005) |
Entry ID: 32235096 |
| OS update with MPI/PROFIBUS |
Entry ID: 19701610 |
|