show the entry list
WinCC flexible ES -- Setting up development environments -- Installing / transferring licenses
What might be the cause for not all the user interface languages being available for selection?
What should you watch out with regard to licenses for WinCC flexible and panels?
Which license do you require for "Historical Data"?
Why isn't it possible with WinCC flexible 2005 to transfer licenses to a SIMATIC Panel PC 477 with embedded operating system?
How can you transfer licenses to an operator device with the ALM without WinCC flexible being installed?
Licensing and Authorization of SIMATIC WinCC flexible 2004
Multi Panel -- Setting up the system -- Installing and upgrading licenses
How can you transfer licenses to an operator device with the ALM without WinCC flexible being installed?
Touch Panel / Operator Panel -- Setting up systems -- Installing and upgrading licenses
How can you transfer licenses to an operator device with the ALM without WinCC flexible being installed?
Mobile Panels -- Setting up the system -- Installing and upgrading licenses
How can you transfer licenses to an operator device with the ALM without WinCC flexible being installed?
ProSave -- ProSave in general -- Working with ProSave
What should you watch out with regard to licenses for WinCC flexible and panels?
How can you transfer licenses to an operator device with the ALM without WinCC flexible being installed?
Which version of Image of the relevant operator panels can be used for the corresponding version of ProTool?
Error message when transferring the Pocket Internet Explorer to a Windows CE Panel with ProSave
How do you backup/restore with a Windows-based panel?
What connections are there between the version designations in WinCC flexible?
How to Backup and restore a program on a text or graphic-based panel?
How do you back transfer the projects of an operator panel and what should you watch out for?
How do you do an operating system update (OS update) on operator panels?
Specification of the installation path for shared files in the standalone installation of ProSave V6.0 SP2
How can you transfer licenses to an operator device with the ALM without WinCC flexible being installed?
Part number:

Instructions:
In order to transfer licenses to an operator panel with the ALM (Automation License Manager) you need a computer on which the ALM and WinCC flexible are installed.

Alternatively, it suffices to install just the ALM in conjunction with ProSave V7.2 and higher.
This combination also activates the "Connect target system" menu item. 


Fig. 01

You can install the ALM as well as ProSave via the Setup menu of the WinCC flexible 2008 Installation CD. Select the relevant options in the Setup menu.

Alternatively, you can download the ALM and ProSave from the Customer Support site.
 

ALM: See Entry ID: 114358
ProSave: See Entry ID: 10347815

Order of installation:

  1. ALM (Automation License Manager)
  2. ProSave V7.2 or higher

 Entry ID:23238814   Date:2009-12-03 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour