show the entry list

C7 6xx -- Product information -- Technical data 
Which panels are certified for shipbuilding? 
Input delay of the technology digital inputs Length Measurement, Reference Point Switch and Latch in CPU 31xC and C7 613/635 
C7-613: Variable lengths greater than 4 bytes 
Which I/O modules can be used with the signal modules? 

Which panels are certified for shipbuilding?Go to beginning
Part number:

Product information
This entry contains all the SIMATIC HMI panels that have a certificate for shipbuilding from the classification societies.

Contents

  1. Information on the shipbuilding certificate
  2. Current HMI panels with shipbuilding certificate
  3. Discontinued HMI panels with shipbuilding certificate

Before installing the panel, note whether the panel is listed in the certificate and whether type-specific changes have to be made. Without such changes the panel does not have a shipbuilding certificate.

1. Information about the shipbuilding certificate
The classification societies are responsible for classifying ships. A ship must be classified before it can sail for the merchant navy and before it can be insured along with its cargo. SIMATIC HMI Panels are certified by the following classification societies.
 
Code Classification society Country
ABS American Bureau of Shipping USA
BV Bureau Veritas France
DNV Det Norske Veritas Norway
GL Germanische Lloyd Germany
LRS LIoyd's Register of Shipping Great Britain
NK Nippon Kaiji Kyokai Japan
PRS Polski Rejestr Statków Poland
RINA Registro Italiano Navale Italy
RMRS Russian Maritime Register of Shipping Russia
CCS China Classification Society China

2. Current HMI panels with shipbuilding certificate
The following panels have been certified by various shipbuilding classification societies.

Note
Note that in some panels, for example, an additional EMC filter or even lightning protection is required for the power supply for these panels to be certified. Details about shipbuilding certification are available in the relevant certificates.

The panels in the table below are currently sold by Siemens.
 
Basic Panels MLFB Link
KTP400 Basic mono 6AV6647-0AA11-3AX0 available certificates
KTP400 Basic color PN 6AV6647-0AK11-3AX0 available certificates
KTP600 Basic mono PN 6AV6647-0AB11-3AX0 available certificates
KTP600 Basic color DP 6AV6647-0AC11-3AX0 available certificates
KTP600 Basic color PN 6AV6647-0AD11-3AX0 available certificates
KTP1000 Basic color DP 6AV6647-0AE11-3AX0 available certificates
KTP1000 Basic color PN 6AV6647-0AF11-3AX0 available certificates
KTP1500 Basic color PN 6AV6647-0AG11-3AX0 available certificates
Comfort Panels MLFB Link
KP400 Comfort 6AV2124-1DC01-0AX0 available certificates
KTP400 Comfort 6AV2124-2DC01-0AX0 available certificates
KP700 Comfort 6AV2124-1GC01-0AX0 available certificates
TP700 Comfort 6AV2124-0GC01-0AX0 available certificates
KP900 Comfort 6AV2124-1JC01-0AX0 available certificates
TP900 Comfort 6AV2124-0JC01-0AX0 available certificates
KP1200 Comfort 6AV2124-1MC01-0AX0 available certificates
TP1200 Comfort 6AV2124-0MC01-0AX0 available certificates
TP1500 Comfort 6AV2124-0QC02-0AX0 Certificates in preparation.
KP1500 Comfort 6AV2124-1QC02-0AX0 Certificates in preparation.
TP1900 Comfort 6AV2124-0UC02-0AX0 Certificates in preparation.
TP2200 Comfort 6AV2124-0XC02-0AX0 Certificates in preparation.
Micro Panels MLFB Code
OP73micro

6AV6640-0B..

available certificates
TP177micro

6AV6640-0CA1..

available certificates
Operator Panel MLFB Code
OP73 6AV6641-0A..
available certificates
OP77A 6AV6641-0B..
available certificates
OP77B 6AV6641-0C..
available certificates
OP177B DP 6AV6642-0DC01-1AX0
available certificates
OP177B PN/DP 6AV6642-0DA01-1AX0
available certificates
OP277 6" 6AV6643-0B..
available certificates
Touch Panels MLFB Code
TP177A 6AV6642-0A..
available certificates
TP177B 4" 6AV6642-0BD01-3AX0
available certificates
TP177B DP 6AV6642-0BC01-1AX..
available certificates
TP177B PN/DP 6AV6642-0BA01-1AX0
available certificates
TP277 6" 6AV6643-0A..
available certificates
Multi Panels MLFB

Code

MP177 6" 6AV6642-0EA01-3AX..
available certificates
MP277 8" Key 6AV6643-0DB01-1AX..
available certificates
MP277 8" Touch 6AV6643-0CB01-1AX..
available certificates
MP277 10" Key 6AV6643-0DD01-1AX..
available certificates
MP277 10" Touch 6AV6643-0CD01-1AX..
available certificates
MP377 15" Touch Daylight 6AV6644-8AB20-0AA1 available certificates
1) Certificates in preparation.

3. Discontinued HMI panels with shipbuilding certificate
The following panels have been certified by various shipbuilding classification societies.

Note
Note that in some panels, for example, an additional EMC filter or even lightning protection is required for the power supply for these panels to be certified. Details about shipbuilding certification are available in the relevant certificates.

The panels in the following table are discontinued and to a certain extent can no longer be procured as new parts.
 
Text Displays (COROS) MLFB Code
TD17 6AV3 017.. available certificates
OP3 6AV3 503.. available certificates
OP5 6AV3 505-1.. available certificates
OP7 6AV3 607-1.. available certificates
OP15 6AV3 515-1.. available certificates
OP17 6AV3 617.. available certificates
Graphics Displays MLFB Code
OP25 6AV3 525.. available certificates
Operator Panel MLFB Code
OP170B 6AV6542-0B.. available certificates
OP270 6" Key 6AV6542-0CA10-0AX.. available certificates
OP270 10" Key 6AV6542-0CC10-0AX0 available certificates
Touch Panels MLFB

Code

TP170A

6AV6 545-0B..

available certificates
TP170B

6AV6 545-0B..

available certificates
TP270 6"

6AV6545-0CA10-0AX..

available certificates
TP270 10"

6AV6545-0CC10-0AX0

available certificates
Multi Panels

MLFB

Code

MP270B 6" Touch 6AV6 545-0A.. available certificates
MP270B 10" Key 6AV6 545-0AG10-0AX0 available certificates
MP270B 10" Touch

6AV6 545-0AG10-0AX0

available certificates
MP370 12" Key

6AV6542-0DA10-0AX0

available certificates
MP370 12" Touch

6AV6 545-0DA10-0AX0

available certificates
MP370 15" Touch

6AV6 545-0DB10-0AX0

available certificates
C7 devices MLFB Zulassung
C7-613

6ES7 613-1CA0..

available certificates

C7-621

6ES7 621-1AD0..

available certificates
C7-623

6ES7 623-1..

available certificates

C7-624

6ES7 624-1..

available certificates
C7-626

6ES7 626-..

available certificates
C7-633

6ES7 633-..

available certificates
C7-634

6ES7 634-..

available certificates
C7-635

6ES7 635-2E..

available certificates
C7-636

6ES7 636-2..

available certificates

Additional Keywords
Classification, Shipbuilding certificate

Input delay of the technology digital inputs Length Measurement, Reference Point Switch and Latch in CPU 31xC and C7 613/635Go to beginning
Part number:

QUESTION:
What is the input delay of the technology digital inputs Length Measurement, Reference Point Switch and Latch in CPU 31xC and C7 613/635?

ANSWER:
The technology digital inputs Length Measurement, Reference Point Switch and Latch have an input delay of 48µs for the technological functions "Count" and "Position".

The associated pin assignments and addresses of these digital inputs are listed below for the CPU/C7 modules.

Note:
For evaluation of these digital inputs as default inputs, the input delays that you have parameterized in the HW Config in the "Inputs" tab in Properties DI/DO.

Reference documentation:
The description is based on the following sections in the manual "CPU 31xC, Technological Functions" (Edition 05.2003), Entry ID. 12429336

Terminals for Positioning with Analog Output

Section 3.1.3

Terminals for Positioning with Digital Output

Section 4.1.3

Terminal Assignment

Section 5.2.2

The C7 devices are described in the following manuals:

SIMATIC C7-613 Control System, Edition: 03/2003

Entry ID 13125532

SIMATIC C7-635 Control System, Edition: 02/2003

Entry ID 11559312

Technology digital inputs:

  • Length measurement and reference point switch
These inputs are evaluated with the "Position" function.
  • The Length Measurement input is for storing the actual value of the position at change of edge.
  • The Reference Point Switch input is for selecting the zero mark signal to be used for synchronization.

Module

Connector

Length Measurement

Reference Point Switch

Pin assignment

Address

Pin assignment

Address

CPU 314C-2 DP / PtP

X2

5

DI +0.3

6

DI +0.4

C7 635

X11

4

DI +0.3

5

DI +0.4

Table 1: Pin assignment and addresses for the Length Measurement and Reference Point Switch inputs

  • Latch
    This input is evaluated with the "Count" function. The Latch input is for storing the counter value in the case of a positive edge.

Module

Connector

Pin assignment

Address

CPU 312C

X1

8 ... 9

DI +0.6 ... DI +0.7

CPU 313C

X2

16 ... 18

DI +1.4 ... DI +1.6

CPU 313C-2 DP / PtP

X1

16 ... 18

DI +1.4 ... DI +1.6

CPU 314C-2 DP / PtP

X2

16 ... 19

DI +1.4 ... DI +1.7

C7 613

X11

13 ... 15

DI + 1.4 ... DI +1.6

C7 635

X11

13 ... 16

DI +1.4 ... DI +1.7

Table 2: Pin assignment and addresses for the Latch inputs


C7-613: Variable lengths greater than 4 bytesGo to beginning
Part number:

QUESTION:  
How can I obtain variable lengths greater than 4 bytes?

ANSWER:  
The variable length is limited to 4 bytes. If you want to display a text with more than 4 characters, for example, you can output the text exceeding the 4 characters with a second variable (and so on as required).


Which I/O modules can be used with the signal modules?Go to beginning
Part number:

Description:
In addition to the signal modules (SM) you can use modules that require communication and connection resources (K bus nodes). In this way you can use all function modules (FM) and communication processors (CP).

 Entry ID:22832385   Date:2013-04-24 
I regard this article....as helpfulas not helpful                                 






























related links
SITRANS R200 Display Recorder - C ...
Process Diagnosis ProAgent for OP
SITRANS R260 Display Recorder - C ...
SITRANS R230 Display Recorder - C ...
SIMATIC S7-300 CPU 31xC Technolog ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour