show the entry list

PROFIBUS network components (electrical/optical) -- Product information -- Technical data and certificates 
To which PROFIBUS Optical Link Module (OLM) can you connect a single-mode or mono-mode glass fiber-optic cable? 
Bus connection with PROFIBUS PA 
OLM with different cable types 
Where can you find information on the the dimensions of PROFIBUS connectors and where can you find dimensioned drawings of the PROFIBUS connectors? 

To which PROFIBUS Optical Link Module (OLM) can you connect a single-mode or mono-mode glass fiber-optic cable?Go to beginning
Part number:

Description
You can connect single-mode or mono-mode glass fiber optic cables (9/125µm or 10/125µm) to the following PROFIBUS Optical Link Modules (OLM):

  • PROFIBUS OLM/G11-1300
  • PROFIBUS OLM/G12-1300

The properties of the single-mode or mono-mode glass fiber optic cable must meet the specifications of the optical interfaces of the OLM.
The optical interfaces of the OLM are BFOC sockets. The following table shows the specifications of the optical interfaces of OLM/G11-1300 and OLM/G12-1300.
 
  OLM/ G11-1300 OLM/G12-1300
Number of optical interfaces 2x BFOC sockets 4x BFOC sockets
Wavelength 1310 nm 1310 nm
Linkable optical transmission power referred to 1mW -19 dB -19 dB
Optical sensitivity referred to 1mW -29 dB -29 dB
Attenuation of the fiber-optic transmission path 8 dB 8 dB
Length of the single-mode or mono-mode glass fiber-optic cable 0 to 15 km 0 to 15 km

Note
More information on the PROFIBUS OLMs is available in the manual

1. PROFIBUS OLM V4.0 in Entry ID 24164176.

Bus connection with PROFIBUS PAGo to beginning
Part number:

QUESTION:
How has the PROFIBUS PA bus to be terminated?

ANSWER:
With a capacitor (C= 1µF) and a resistor (R = 100 Ohm) in series between data lines A and B (pins 3 and 8).

Keywords:
Service

OLM with different cable typesGo to beginning
Part number:

QUESTION:
Can an OLM work with different plastic fiber- as well as quartz glass- fiber cable types?

ANSWER:  
No. An OLM does only support one cable type, not several ones at the same time.

Note:
Further information regarding OLM is available in the manual "SIMATIC NET PROFIBUS Optical Link Module" under entry ID 8331164.

Where can you find information on the the dimensions of PROFIBUS connectors and where can you find dimensioned drawings of the PROFIBUS connectors?Go to beginning
Part number:

Description
This entry contains information about the dimensions of the PROFIBUS connectors.
Below are the dimensioned drawings of the PROFIBUS connectors with reference to the order numbers concerned.

Note
The Siemens I IA&DT picture database contains 2D and 3D data of the connectors which you can download free of charge. This gives you the possibility of incorporating the connectors in your CAx system.

I IA&DT picture database

Additional keywords
RS485, Connectors, Sub-D

 Entry ID:22791648   Date:2012-03-14 
I regard this article....as helpfulas not helpful                                 






























related links
Pointek CLS300 - Quick Start Manual
SIMATIC NET PROFIBUS Networks
Pointek CLS 200 (analog/digital) ...
SIMATIC NET PROFIBUS Networks
Pointek CLS300 - Quick Start Manual
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour