show the entry list
3UF57 PCS7-FB SIMOCODE-DP: Compatibility with PCS 7 versions ….
Part number:

QUESTION:

Is there a table for the compatibility with the PCS 7 versions and the SIMOCODE-DP PCS 7 function block?

 

 

ANSWER:

In the following table you find the compatibility of PCS 7 versions and the SIMOCODE-DP PCS 7 function block. 

 

 

3UF5_PCS7_COMPATIBILITY.pdf (60 KB) ( 64 KB )

 

 Entry ID:22578851   Date:2012-05-10 
I regard this article....as helpfulas not helpful                                 
related links
3UF7 SIMOCODE pro: Can the PCS7 ...
Service Pack 2 for PCS7 function ...
3UF5: PCS7-FB SIMOCODE : The setu ...
3UF5: PCS7-FB SIMOCODE: How can t ...
Service Pack 2 (SP2) for PCS 7 SI ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour