Configuration Notes: WinAC ODK (Open
Development Kit) V4.1 is required for a PC application which
has been developed with WinAC Slot T-Kit (and used with WinAC Slot
PLC) and which you also wish to use with WinAC Basis Soft PLC or
WinAC RTX.
WinAC ODK V4.1 is an engineering software
package for the development of PC applications in connection with
WinAC Basis V4.1, WinAC RTX V4.1 and WinAC Slot V3.4. This software
supports the integration of PC software using C/C++ for WinAC
software and Slot PLC.
You can find further information on the Internet in Entry ID
19020768 (WinAC ODK V4.1 available immediately).
This configuration has been verified with a WinAC Basis
V4.1.
|