|  |
The memory expansion cartridge can be used
for:
- SIMATIC Box PC
627 (order no.: 6ES7647-6M...)
- SIMATIC Panel PC
677 (order no.: 6AV780...)
- SINUMERIK
PCU50.3 (order no.:
6FC5210-0DF3...)
The
memory cartridge has been tested and released for the above
systems. Memory upgrading is a drastic system modification and
should only be performed with released memory cartridges to ensure
that the functionality of the PC is maintained.
Ordering data:
|
Order No.
(MLFB) |
Designation |
|
6ES7648-2AG40-0GA0 |
SIMATIC PC
MEMORY EXPANSION,
1 GBYTE, DDR2 533, SODIMM;
BOX PC 627, PANEL PC 677,
PCU50.3 |
The
new memory cartridge will also be listed in the SIMATIC PC
configurator for SIMATIC Box PC 627 and SIMATIC Panel PC 677. PC
configurations with up to 2 Gbytes are now available for
memory-intensive applications.
|  |  |