show the entry list
WinCC flexible ES -- Working with projects -- Creating, editing, archiving and copying projects
What do you have to do if you can no longer access symbols and data blocks of STEP 7 from an integrated WinCC flexible project?
Which entries are available on the internet for migration to STEP 7 (TIA Portal) and WinCC (TIA Portal)?
How can you change the column width of picture objects in WinCC flexible?
In WinCC flexible, how can you prevent pictures and picture objects being fitted automatically when you change the screen resolution (possibly widescreen)?
How do you activate access protection for a STEP 7 project and set up a user as project editor?
How do you integrate a WinCC flexible project in STEP 7?
How can you use one and the same WinCC flexible operator panel configuration for multiple controllers?
What are the solutions offered for working with different versions of WinCC flexible?
Which problems might arise if the "log.LDF" file is not available in a WinCC flexible project?
Why does WinCC flexible close again automatically after the program start?
How do you save WinCC flexible projects / libraries in the format of an earlier version of WinCC flexible?
How can you delete unused tags or objects from a WinCC flexible project?
What options do you have for copying pictures from one WinCC flexible project to another?
Copying HMI projects integrated in SIMATIC STEP 7 at file level
How can you open a WinCC project integrated in STEP 7 faster?
How do you archive projects in WinCC flexible and which files are required?
How do you back transfer the projects of an operator panel and what should you watch out for?
Which connector cables are available for connecting to SIMATIC Panels?
ProSave -- ProSave in general -- Working with ProSave
What should you watch out with regard to licenses for WinCC flexible and panels?
How can you transfer licenses to an operator device with the ALM without WinCC flexible being installed?
Which version of Image of the relevant operator panels can be used for the corresponding version of ProTool?
Error message when transferring the Pocket Internet Explorer to a Windows CE Panel with ProSave
How do you backup/restore with a Windows-based panel?
What connections are there between the version designations in WinCC flexible?
How to Backup and restore a program on a text or graphic-based panel?
How do you back transfer the projects of an operator panel and what should you watch out for?
How do you do an "Operating system update" (OS update) or "Reset to factory settings" on operator panels?
Specification of the installation path for shared files in the standalone installation of ProSave V6.0 SP2
Text display / Graphics devices -- Creating HMI configurations -- Transferring projects
How do you back transfer the projects of an operator panel and what should you watch out for?
Micro Panels -- Setting up systems -- Transferring projects
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?
Which connector cables are available for connecting to SIMATIC Panels?
How do you back transfer the projects of an operator panel and what should you watch out for?
Mobile Panels -- Setting up systems -- Transferring projects
In WinCC (TIA Portal), how do you transfer a project to an HMI panel using S7 Routing when the CPU has been programmed with STEP 7 V5.5?
Why can you not transfer the HMI configuration to the panel?
With WinCC Engineering (TIA Portal), how can you transfer an HMI configuration without configuration software to an operator panel (Pack&Go)?
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS?
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?
Which connector cables are available for connecting to SIMATIC Panels?
How do you back transfer the projects of an operator panel and what should you watch out for?
How do you simulate the system keyboard via K or F-keys?
How can you transfer a WinCC flexible project via Ethernet to a Windows-based panel?
Touch Panel / Operator Panel -- Setting up systems -- Transferring projects
Why can you not transfer the HMI configuration to the panel?
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS?
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?
Which connector cables are available for connecting to SIMATIC Panels?
How do you back transfer the projects of an operator panel and what should you watch out for?
Transferring the configuration in the case of graphics-oriented devices
Transferring a configuration with Windows-based devices
How do you simulate the system keyboard via K or F-keys?
How can you transfer a WinCC flexible project via Ethernet to a Windows-based panel?
Screen disabling with OP27 and TP27
Configuring headers of OP3 pictures in ProTool V5.2 /SP2
When editing the second OP language, variables are shifted in the other language.
Multi Panel -- Setting up systems -- Transferring projects
Why can you not transfer the HMI configuration to the panel?
With WinCC Engineering (TIA Portal), how can you transfer an HMI configuration without configuration software to an operator panel (Pack&Go)?
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS?
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?
Which connector cables are available for connecting to SIMATIC Panels?
How do you back transfer the projects of an operator panel and what should you watch out for?
How do you simulate the system keyboard via K or F-keys?
How can you transfer a WinCC flexible project via Ethernet to a Windows-based panel?
How do you back transfer the projects of an operator panel and what should you watch out for?
Part number:

Contents:
In this FAQ we describe how to back transfer projects, which operator panels support this function and what you should pay attention to.

Please follow the instructions in the PDF file (Attachment 1).
The following points are covered in the document.

1. General Information
    1.1 Using back transfer
    1.2 Advantages of back transfer
    1.3 Requirements for back transfer

2. Procedure
    2.1 Project transfer and back transfer

3. Frequently Asked Questions
    3.1 Why is the message "Could not find the pdz file" displayed?
    3.2 How do you determine whether a back-transferred file is on the panel?

Attachment 1: Back_transfer_description_e.pdf ( 491 KB )

Requirements for back transfer
Attachment 2 lists the operator panels and indicates which HMI software is required to transfer projects and which operator panels permit back transfer of the configuration file from the operator panel.

Furthermore it also shows from which operator panels you can do a backup/restore via ProSave and which operator panels permit backup/restore to/from external memory cards.

Attachment 2: Back_transfer_devices_e.pdf ( 60 KB )

Note:
A comparable method of saving projects is with Backup/Restore. More information on this topic is available in the following Entry IDs: 28928853, 26588748 and 213262.

Keywords:
Panel, WinCC flexible, Store, 13393218, 5672699

 Entry ID:21907703   Date:2012-01-02 
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
Themen
Help
Online Help
Guided Tour