show the entry list
ES - SIMATIC Manager -- Product information -- Checking compatibility
Compatibility Tool for Automation and Drive Technology
What are the basic requirements for data exchange between COMOS and SIMATIC PCS 7?
Why should you not install the Microsoft security patches KB2467174, KB2467175, KB2465361 and KB2465367 in WinCC, PCS 7 and WinCC Professional V11?
How can you find out which Microsoft Patches are installed on the PC?
Why can different versions of PCS 7 not be operated in mixed mode?
Which modules and their firmware versions are released for PCS 7 and how can you upgrade them?
With what are SIMATIC PCS 7 V8.x, V7.x, V 6.x, V5.x and V4.x compatible?
Why can't you use Service Packs for Microsoft Windows, the MS SQL Server or the Internet Explorer if they do not originate from the CDs/DVD provided with the PCS 7 software?
What support does Microsoft provide for Microsoft products (operating systems and Internet Explorer) implemented with PCS 7?
Which Microsoft Patches ("Security Patches" and "Critical Patches") have been tested for compatibility with SIMATIC PCS 7?
Important note on Microsoft Patches KB 943459 and KB 971468
Important note when using Microsoft's automatic update service in PCS 7.
Additional information on the compatibility of PCS 7 V6.x and Microsoft products
Important note when using Microsoft's automatic update service in PCS 7.
Part number:

Instructions:

Important note when using Microsoft's automatic update service in PCS 7.

The automatic update service must be disabled with SIMATIC PCS 7!

If the update service is enabled, there is a danger that new software packages, service packs, hotfixes etc. will be installed by Windows components, which under certain circumstances might cause problems with PCS 7 if the constellation has not yet been tested and officially released.
New packages issued by Microsoft should only be installed after thorough testing for compatibility (e.g. with reference to the PCS 7 Release Notes).

Option 1 for disabling:
You can disable the automatic update service if necessary in the Control Panel by double-clicking on the "Automatic Updates" icon and deselecting the relevant option.

Option 2 for disabling:
By disabling the "Automatic Updates" service under:

  • "Computer Management > Services and Applications > Services" or
  • "Start > Settings > Control Panel > Administration > Services > "Automatic Updates"

Note:
The SIMATIC Rack PC IL 40 S was supplied for a time with "Restore" Images in which the Microsoft automatic update service is enabled. You must disable this after a "Restore".

You must make special arrangements for the following system configurations:
 
No. System configuration
1 Central software update server for office and system networks
If you are using a common SUS for your office network and the PCS 7 system network, which automatically receives the updates from the Microsoft servers and automatically distributes these to the PCs in the office and PCS 7 system networks, you must make sure that the PCS 7 system PCs do not receive these software updates!
2 Automatic update service enabled on the PCS 7 system PCs upon access to the Internet
If your PCS 7 system PCs have a direct Internet access and the automatic update service is started on these PCs, then please disable the automatic update service or make sure that the PCS 7 system PCs do not have a direct Internet access!

Therefore we recommend that either you install the Microsoft Security Patches manually or you assign the updates to the various networks via a dedicated software update server.

Note:
In the case of the PC bundles released for PCS 7 V6.1 in the ST PCS 7 catalog, the automatic update service is disabled by default for security reasons. Please note that this automatic update service is switched on in most other PCs!

Keywords:
Upgrading, Hotfix, Service Pack, SP, HF

 Entry ID:21394429   Date:2009-11-17 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour