Description
The document attached for downloading contains information on the topic of
USB transfer.
- Tested USB cables
- Released operator panels
- Installation of the USB driver
- Making a transfer to an operator panel via USB
- Possible error messages and how to clear the errors
Note
Please bear in mind that over the course of time manufacturers/suppliers change their product or order designations, offer new versions of products or discontinue products from their range. Successor products are not necessarily suitable for transfer!
Attachment 1: USB_Transfer_V1_0_e.pdf ( 726 KB )
Keywords
Project transfer, Transfer, USB driver, USB Master-Master, Lindy, 22408158
|