show the entry list
Changing the firmware version of a Masterdrives in a Step7 project.
Part number:

QUESTION:
Masterdrives was connected on the Profibus via DriveES-OM from the Hardware catalog in a Step7 project. What changes need to be made in the project if the firmware of a Masterdrives is changed.

ANSWER:
Call the drive properties of the drive in the project path (right mouse button on motor icon ==> Object Properties, Drive tab). Select the new firmware version there. The help under "Changing device version" (Changing drive version) describes how to proceed. In particular, drives with non-empty parameter containers can only be changed to higher firmware version.

 Entry ID:16626566   Date:2003-09-29 
I regard this article....as helpfulas not helpful                                 
related links
SINAMICS DCM, Application: Load-b ...
SIMATIC S7 S7-1200 Programmable c ...
SIMOTION SIMOTION D4x5-2
STEP 7 Professional V11.0 SP1
DriveMonitor, script files for di ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour