show the entry list
WinCC -- Product information -- System description
Which Details does Technical Support need regarding Inquiries on SIMATIC WinCC
Which user rights does a user have who belongs to multiple Windows user groups of which several are stored in the WinCC User Administrator?
Further information on the Catalog ST80 with regard to WinCC Communication
SIMATIC WinCC on PCs with AMD-Processors
How can you use the license for Microsoft SQL Server 2000 in conjunction with WinCC?
WinCC -- Working with projects -- Analyzing error messages
Which Details does Technical Support need regarding Inquiries on SIMATIC WinCC
Why is the message "Network not ready yet." displayed when an AutoStart is configured on the OS?
Why do you get the error message "Not enough server memory available for this command."?
Why is it not possible to open or use WinCC editors or why can you only open the project as write-protected?
Why do you get the message "Open WinCC project: The user does not have the rights to perform this action!"?
Why are error messages displayed when creating the CrossReference in WinCC?
Why do you get the "Server not available" message when you attempt to open the project from the client?
When shutting down Windows NT, why do you get the error message saying that other users are accessing the project database?
Why, after upgrading from WinCC V5.0 SP1 to SP2 doesn't ISQL access to the Runtime database no longer work?
Why can't you create any pictures and scripts in WinCC?
WinCC -- Operation and maintenance -- Diagnosing errors
How do you install the User Mode Process Dumper for diagnostics with WinCC and PCS 7?
Which Details does Technical Support need regarding Inquiries on SIMATIC WinCC
When you open an image in RT or when you click a user object, why is an "OnErrorExecute" generated and why is the faceplate not displayed?
How can you increase the timeout for starting and terminating Alarm Logging / Tag Logging?
Which tools does WinCC Scope offer for diagnosis and system information?
How can you clear the cause for the message "StgOpenStorage hr= 80030002 ..." when working with the Graphics Designer?
Why is the error message "Open WinCC project - The project cannot be opened before it's converted with Project Migrator" displayed when opening a WinCC project?
What is the meaning of the following entry in the WinCC diagnostics file WinCC_Sys_xx.log: "DataManager Runtime, Update data lost, ..."?
What can be the cause of the message "HResult Error" in conjunction with WinCC?
Why does SIMATIC WinCC V6.0 not start or why does it stop with an HResult error?
Why does WinCC V5 crash in Runtime with pcAnywhere V8.0/8.01?
Which Details does Technical Support need regarding Inquiries on SIMATIC WinCC
Part number:

QUESTION:  
Which Details does Technical Support need regarding Inquiries on SIMATIC WinCC?

ANSWER:  
For the Technical Support to reply to an inquiry precisely and without questions, a description as precise as possible of the facts to be clarified is necessary..

This entry contains a compilation of FAQs from the area of SIMATIC WinCC and a list of the information required by Technical Support.

In any event, the following information is absolutely essential for ensuring that a CPU-related query can be processed speedily:

  • SIMATIC WinCC version (version, service pack, Hotfix, WinCC options, WinCC add-ons),
  • Configuration or topology of the system (server, clients, PLC),
  • Details about the operating system (version, service pack, Internet Explorer),
  • Details about additional software installed (SIEMENS or non-SIEMENS software).

In addition to the general details, the following section summarizes the additional information required for FAQs:

1. Query about the configuration
2. License error message
3. Communication problems
4. Error messages from WinCC Runtime components
5. Performance optimization
6. TIA - (Totally Integrated Automation)

1. Query about the configuration
The details specified above and a concrete description of the required functions are sufficient for queries on the configuration.

2. License error message

  • Screenshot of the installed authorizations on the computer in question ("Simatic > AuthorsW > AuthorsW").
  • "License.log" and "License.bak" files (if present) from the "Siemens\WinCC\Diagnose" folder.

3. Communication problems

  • Information about clients/servers in question, status in life beat monitoring or connection status in WinCC Explorer under "Options > Connections Status".
  • SIMATIC NET version, as well as the type and description of the communication modules used. 
  • Send us the diagnostic files from Siemens\WinCC\Diagnose on the server and from the client (in compressed format, if possible, e.g. as a *.zip archive).
  • Send us the event log from Microsoft Windows NT/2000/XP if problems arise with the communication card in the computer (refer to Entry ID 15386411 for details about the procedure).

4. Error messages from WinCC Runtime components

  • Send us all the files from the "Siemens\WinCC\Diagnose" folder.
  • Send us the event log from Microsoft Windows NT/2000/XP if problems arise with the communication card in the computer (refer to Entry ID 15386411 for details about the procedure).
  • In the case of Microsoft Windows NT 4.0/2000/XP, send us Drwtsn32.log and the backup of User.dmp (if they are present and not too big).
  • As precise a description of the fault as possible.
  • If possible, screenshots showing any error messages that are displayed.

5. Performance optimization

  • Precise details about the computer hardware: processor type, RAM, hard disk capacity (free memory capacity).

6. TIA - (Totally Integrated Automation)

  • List of the installed SIMATIC software in the form of a csv file. This is created in the SIMATIC Manager via "Help > Info > Installed Software: Display".

Please also note Entry-ID: 18194667 for the exchange of files with Technical Support.

In order to submit an inquiry to the technical support, please use the link " Requesting Technical Support (Support Inquiry)" at the end of the entry.

Keywords:
Technical Support, Hotline, Information, Help, Problem, Customer Support, Prerequisites


 Entry ID:16607894   Date:2003-08-01 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour