show the entry list
DriveES Graphic, copying charts.
Part number:

QUESTION:  
A Masterdrives CUVC, V3.3 with DriveES interface is inserted in a Step7 project. A chart folder is set-up below this. I now wish to copy one of the charts from the project example of the DriveES Graphic CD into an empty chart folder. That doesn't work. The error message says that 162 blocks were not able to be copied.

The same behavior occurs for a Masterdrives MC V1.6.

ANSWER:  
Charts can only be copied if they are generated in the same language. The project examples are in English so that it is not possible to copy them into a "German" chart.

After opening the chart, in CFC, it is possible to change the language used when setting-up blocks. This is also explained in the first sheet of partial chart A in the project example in a command window.

 Entry ID:13739550   Date:2002-11-25 
I regard this article....as helpfulas not helpful                                 
related links
SIMATIC Process Control System PC ...
CFC for S7 Continuous Function Chart
SIMATIC CFC for S7 Continuous Fun ...
CFC for S7 V6.1
Blocks in flowchart cannot be deleted
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Themen
Help
Online Help
Guided Tour