show the entry list
C7 6xx -- Product information -- Technical data
Which panels are certified for shipbuilding?
Input delay of the technology digital inputs Length Measurement, Reference Point Switch and Latch in CPU 31xC and C7 613/635
C7-613: Variable lengths greater than 4 bytes
Which I/O modules can be used with the signal modules?
S7-300 CPU 31xC -- Using Technology -- Information to integrated functions of CPU31xC
Why does the counter value always jump between 0 and 1 when using a 24-volt encoder?
Why is it not possible to load blocks from the Standard Library "S5-S7 Converting Blocks" into a CPU 312C?
How can you increase the resolution of temperature measurements using PT100 via the integrated analog input of the CPU 31x C?
CPU 31xC: Reading Inputs
CPU 314C-2PtP: failure when positioning with analog output in JOG mode
Where are the cabling diagrams for S7-300 compact CPUs located?
Configuring the "Signal evaluation:" parameter in 31xC CPUs using the technological function "Count"
Use of input and output of CPU 31xC by the technological function count and as "normal" Input and output
Input delay of the technology digital inputs Length Measurement, Reference Point Switch and Latch in CPU 31xC and C7 613/635
DO outputs of a compact CPU are destroyed
Input delay of the technology digital inputs Length Measurement, Reference Point Switch and Latch in CPU 31xC and C7 613/635
Part number:

QUESTION:
What is the input delay of the technology digital inputs Length Measurement, Reference Point Switch and Latch in CPU 31xC and C7 613/635?

ANSWER:
The technology digital inputs Length Measurement, Reference Point Switch and Latch have an input delay of 48µs for the technological functions "Count" and "Position".

The associated pin assignments and addresses of these digital inputs are listed below for the CPU/C7 modules.

Note:
For evaluation of these digital inputs as default inputs, the input delays that you have parameterized in the HW Config in the "Inputs" tab in Properties DI/DO.

Reference documentation:
The description is based on the following sections in the manual "CPU 31xC, Technological Functions" (Edition 05.2003), Entry ID. 12429336

Terminals for Positioning with Analog Output

Section 3.1.3

Terminals for Positioning with Digital Output

Section 4.1.3

Terminal Assignment

Section 5.2.2

The C7 devices are described in the following manuals:

SIMATIC C7-613 Control System, Edition: 03/2003

Entry ID 13125532

SIMATIC C7-635 Control System, Edition: 02/2003

Entry ID 11559312

Technology digital inputs:

  • Length measurement and reference point switch
These inputs are evaluated with the "Position" function.
  • The Length Measurement input is for storing the actual value of the position at change of edge.
  • The Reference Point Switch input is for selecting the zero mark signal to be used for synchronization.

Module

Connector

Length Measurement

Reference Point Switch

Pin assignment

Address

Pin assignment

Address

CPU 314C-2 DP / PtP

X2

5

DI +0.3

6

DI +0.4

C7 635

X11

4

DI +0.3

5

DI +0.4

Table 1: Pin assignment and addresses for the Length Measurement and Reference Point Switch inputs

  • Latch
    This input is evaluated with the "Count" function. The Latch input is for storing the counter value in the case of a positive edge.

Module

Connector

Pin assignment

Address

CPU 312C

X1

8 ... 9

DI +0.6 ... DI +0.7

CPU 313C

X2

16 ... 18

DI +1.4 ... DI +1.6

CPU 313C-2 DP / PtP

X1

16 ... 18

DI +1.4 ... DI +1.6

CPU 314C-2 DP / PtP

X2

16 ... 19

DI +1.4 ... DI +1.7

C7 613

X11

13 ... 15

DI + 1.4 ... DI +1.6

C7 635

X11

13 ... 16

DI +1.4 ... DI +1.7

Table 2: Pin assignment and addresses for the Latch inputs


 Entry ID:12894864   Date:2003-09-08 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour