|
QUESTION:
When installing Drive ES Basic remains frozen at a specific
location and does not continue. For the "Register application" this
is 68% after an installation progress.
ANSWER:
This involves the same behavior/response as has been described
under Article ID 8360961.
The configuring tool for the FM357-2 is installed on the computer.
This installs write protected files on the computer. Other setups
attempt to access these write-protected files and therefore run in
an endless loop.
The files involved are in the following folder
"[LW]:\SIEMENS\STEP7\s7reg".
Remedy:
In order to resolve this behavior, for the files involved, the
write protection must be removed under "Properties" or all of the
files deleted in the folder "[LW]:\SIEMENS\STEP7\s7reg". However,
only delete the files in this folder !
Then, all of the following setups can be executed without any
problem.
|